Recently searched
      • Published 22 Feb 2024
      • Last Modified 6 Mar 2024
    • 5 min

    Three Key Factors for Choosing the Right Ammeter

    Discover the key factors for choosing the right ammeter for industrial and electrical applications - application, ease of use, and durability.

    RS marketing banner

    Selecting the right ammeter is crucial in ensuring accurate and reliable measurements in Australia’s industrial and electrical applications. An ammeter, a device used to measure electric current, is a fundamental parameter in any electrical system, and its accuracy is vital for a safe and efficient system operation.

    Whether for routine monitoring, diagnostic purposes, or critical measurements in high-stakes environments, the choice of an ammeter can impact the outcome. In this blog, we explore what does the ammeter measure and the key factors to selecting the right one for professional use in industrial and commercial settings.

    Three Key Factors for Choosing the Right Ammeter

    1. Application

    The application of an ammeter is a primary consideration that shapes its features and functionalities. In Australia’s industrial settings, where equipment often operates under high loads for extended periods, ammeters need to be robust and capable of handling large current ranges without compromising accuracy. These environments may also demand ammeters that can withstand external influences like electromagnetic interference, vibrations, and temperature fluctuations.

    In contrast, laboratory environments prioritise precision and the ability to measure small current variations accurately. The choice here leans towards ammeters that offer high resolution and stability over time. For field testing and on-site diagnostics, portability becomes a crucial factor. Lightweight, compact ammeters with user-friendly interfaces are preferred, allowing technicians to conduct measurements efficiently in various locations.

    At the same time, matching the ammeter to the application involves a careful assessment of its range, accuracy, and type. Digital ammeters, known for their precise readings and ease of interpretation, are often favoured in environments where data accuracy is paramount.

    Meanwhile, with their real-time needle movement, analogue ammeters are still valued in specific applications for their quick response and ability to show trends over time. Similarly, clamp ammeters offer the convenience of measuring current without direct contact with the conductor, making them ideal for quick checks and troubleshooting in field settings.

    2. Ease of Use

    Another factor to consider when choosing the right ammeter is the ease of use, particularly in scenarios where time efficiency and quick assessments are necessary. The physical size and design of the ammeter play a significant role, especially in field applications where portability is key.

    For instance, handheld ammeters that are lightweight and ergonomically designed make it easier for technicians to carry and use them in various environments, from cramped industrial sites to outdoor settings.

    The advent of digitalisation in measurement tools has also introduced features like data logging and connectivity, which are becoming increasingly important. Modern ammeters equipped with data logging capabilities allow for the recording of measurements over time, facilitating trend analysis and long-term monitoring.

    Additionally, connectivity features like USB or wireless interfaces enable seamless data transfer to computers or cloud-based systems for further analysis. This integration with software and data analysis tools enhances the utility of the ammeter, making it a versatile instrument for comprehensive electrical system analysis.

    3. Durability

    Aside from the ease of use and type of ammeter application, durability is paramount, especially for ammeters used in industrial and outdoor applications. The ammeter’s build quality, materials used, and design indicate its ability to withstand tough conditions.

    For instance, an ammeter constructed with high-quality materials and robust design is more likely to endure the rigours of industrial environments, including dust, moisture, and mechanical stress exposure.

    The internal components of the ammeter also contribute to its overall durability. High-quality components that resist wear and tear ensure that the ammeter not only withstands physical challenges but also maintains its measurement accuracy over time.

    Besides, this durability aspect is essential for ensuring consistent and reliable performance, a critical requirement in industrial applications where precision is non-negotiable.

    Durability

    Select the Right Ammeter with RS

    When choosing an ammeter, it's essential to consider its application, ease of use, durability and adherence to industrial regulations such as the Civil Aviation Safety Authority’s regulations for ammeter installation. These factors collectively determine the suitability of an ammeter for your specific needs, whether in an industrial setting, a laboratory, or out in the field.

    Reflecting on these key aspects ensures that you select an ammeter that not only measures electric current effectively but also aligns seamlessly with your operational requirements.

    For those searching for a digital amp meter, an analogue ammeter, or any other type of amp meter, RS Australia offers a diverse range of ammeters to fit various industrial applications. Browse our selection of suppliers to find an ammeter that meets your needs, ensuring accuracy, reliability, and efficiency in all your electrical measurements.

    Popular Ammeter Suppliers

    Socomec Ammeters

    Socomec

    Specialising in power switching, monitoring, and energy storage, Socomec's ammeter product range is a testament to its commitment to excellence and sustainability. With a strong focus on ensuring energy efficiency and reliability, their offerings are particularly suited for demanding industrial environments.

    HOBUT Ammeters

    HOBUT

    With a history steeped in innovation and quality, HOBUT is dedicated to providing solutions that ensure accuracy and durability. Their range includes high-quality digital and analogue ammeters, current transformers, and a variety of electrical measuring instruments.

    Siemens Ammeters

    Siemens

    Siemens offers an extensive range of ammeter products that epitomise innovation and quality. As a leader in the industry, Siemens is synonymous with engineering excellence, pioneering some of the most advanced and reliable electrical components on the market.

    Related links